Device-defined data types

Device-defined data types

Device defined data types are listed for these devices:
  • 1756-IF8I
  • 1756-OF8I
  • 1756-IRT8I
  • 1756-IR12
  • 1756-IT16
1756-IF8I analog input device
This table displays the data types for the devices according to the
Connection
selection in
Device definition
.
Connection
Input Data Type
Output Data Type
Configuration Data Type
Input Data (default)
AB:1756_IF8I:I:0
AB:1756_IF8I:O:0
AB:1756_IF8I:C:0
Listen Only
AB:1756_IF8I:I:0
N/A
N/A
1756-IRT8I analog input device
This table displays the data types for the devices according to the
Connection
selection in
Device definition
.
Connection
Input Data Type
Output Data Type
Configuration Data Type
Input Data (default)
AB:1756_IRT8I:I:0
AB:1756_IRT8I:O:0
AB:1756_IRT8I:C:0
Listen Only
AB:1756_IRT8I:I:0
N/A
N/A
1756-IR12 high density temperature input device
This table displays the data types for the devices according to the
Connection
selection in
Device definition
.
Connection
Input Data Type
Output Data Type
Configuration Data Type
Input Data (default)
AB:1756_IR12:I:0
N/A
AB:1756_IR12:C:0
Listen Only
AB:1756_IR12:I:0
N/A
N/A
1756-IT16 high density temperature input device
This table displays the data types for the devices according to the
Connection
selection in
Device definition
.
Connection
Input Data Type
Output Data Type
Configuration Data Type
Input Data (default)
AB:1756_IT16:I:0
N/A
AB:1756_IT16:C:0
Listen Only
AB:1756_IT16:I:0
N/A
N/A
1756-OF8I analog output device
This table displays the data types for the devices according to the
Connection
selection in
Device definition
.
Connection
Input Data Type
Output Data Type
Configuration Data Type
Output Data (default)
AB:1756_OF8I:I:0
AB:1756_OF8I:O:0
AB:1756_OF8I:C:0
Listen Only
AB:1756_OF8I:I:0
N/A
N/A
Redundant Owner
AB:1756_OF8I_RedundantOwner:I:0
AB:1756_OF8I_RedundantOwner:I:0
AB:1756_OF8I:C:0
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal