Transition to Run mode behavior

Transition to Run mode behavior

Most device properties may change while online and while in these modes:
  • Program
  • Remote Program
  • Remote Test (if supported)
  • Remote Run
When the controller is switched from Remote to Run mode:
  • All device properties, with the exception of the
    Description
    box, become read-only.
  • All device properties that contain an unapplied, edited value, revert to the unedited value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.