- Stratix device properties
Create or edit an EtherChannel group
Use the
EtherChannels
view to create a new EtherChannel group or edit an existing EtherChannel group.Prerequisites
- The device is online.
To create a new EtherChannel group or edit an existing EtherChannel group
- On the tab for the device, selectEtherChannels.
- In theEtherChannelsview, do one of these two actions as needed:
- To create a new EtherChannel group, select
.
- To edit an existing EtherChannel group, select
.
- InAdd/Edit EtherChannel, configure these parameters:
- EtherChannel
- Channel Mode
- Port Members
- SelectSetto send the settings to the switch.
Provide Feedback