Enable time synchronization

Enable time synchronization

Use the
Time Sync Configuration
view to enable time synchronization for the switch.
Prerequisites
  • The device is online.
To enable time synchronization
  1. On the tab for the device, select
    Time Sync Configuration
    .
  2. In the
    Time Sync Configuration
    view, select the type of clock, and then configure the resulting parameters.
  3. Select the checkbox for the port you want to enable Time Sync, and then select
    Set
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.