- Stratix device properties
Enter a password
Use the
Enter password
dialog box to enter the password to the switch. The password prevents changes to the configuration of the device by unauthorized personnel.You must enter a password to set the configuration settings, reset the switch, and save and restore a configuration. If the password is invalid, an error message appears.
TIP:
The password must not include embedded spaces.
To enter a password
- InEnter password, in thePasswordbox, enter a valid password, and then selectOK.TIP:The password includes up to 63 characters and is case sensitive. Valid characters include:
- Letters A...Z (upper and lower case)
- Numerals 0...9
- Symbols ` ~ ! @ # $ % ^ & * ( ) _ + , - = { } | [ ] \ : ; ? / .
Provide Feedback