Refresh communication with the switch

Refresh communication with the switch

Refresh
becomes available in the views to allow you to manually refresh the data from the switch as needed.
TIP:
If you made changes to the data on the tab for the device, write the data to the switch before refreshing communication. Any changes not written to the device are lost if you refresh communication before selecting
Set
.
To refresh communication with the switch
  • On the tab for the device, in the view in which you are viewing information, select
    Refresh
    . The latest data from the switch is retrieved and displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.