Reset the PRP diagnostic counters

Reset the PRP diagnostic counters

When needed to assist in troubleshooting issues, reset the diagnostic counters for the PRP nodes using
Reset Counters
in the
Channel Group 1
and
Channel Group 2
views.
TIP:
Reset Counters
is available when online and Link Redundancy Entity is enabled.
To reset the PRP diagnostic counters
  1. On the tab for the device, expand
    Parallel Redundancy Protocol
    , and then select
    Channel Group 1
    or
    Channel Group 2
    depending which diagnostic counters need resetting.
  2. In the
    Channel Group X
    view, select
    Reset Counters
    .
    Sets the PRP counter values to zero and then refreshes the values in the view with the current counter values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.