- Stratix device properties
Starting Public IP Address
If the
Type of Entry
is Subnet
, Starting Public IP Address
must correspond to the size of the subnet mask as shown in this table.Subnet Mask | Starting Public IP Address |
---|---|
255.255.0.0 | The last two octets must be 0. EXAMPLE: 10.200.0.0 |
255.255.255.0 | The last octet must be 0. EXAMPLE: 10.200.1.0 |
255.255.255.128 | The last octet must be 0 or 128. EXAMPLE: 10.200.1.0 or 10.200.1.128 |
255.255.255.192 | The last octet must be one of these numbers:
EXAMPLE: 10.200.1.64 |
255.255.255.224 | The last octet must be one of these numbers:
EXAMPLE: 10.200.1.32 |
255.255.255.240 | The last octet must be one of these numbers:
EXAMPLE: 10.200.1.16 |
Provide Feedback