- Stratix device properties
Transition to Run mode behavior
Most device properties may change while online and while the controller is in the Remote Run mode.
When the controller is switched to Run mode:
- All device properties, with the exception of theDescriptionbox, become read-only.
- All device properties that contain an unapplied, edited value, revert to the unedited value.
Provide Feedback