- Stratix device properties
Device Information view parameters
The
Device Information
view includes these parameters:Parameter | Description |
---|---|
Identification | Displays the device information:
|
Major/Minor Fault Status | Displays the major and minor fault status values:
|
Configured | Displays the switch configuration values:
|
Owned | Displays a yes or no value indicating whether there is an I/O connection. |
Device Identity | Displays Match or Mismatch , indicating the physical device agrees or not agrees with what is specified in the Overview view.This parameter does not take into account the Electronic Keying or Minor Revision selections for the device as specified in the Overview view. For the Match condition to exist, these must agree:
|
Refresh | Retrieves and displays the latest values from the device. |
Reset Device | Initiates a reset operation (power cycle) with the current configuration file. Tip : The Password confirmation dialog box may appear. |
Provide Feedback