- Stratix device properties
Add/Edit Ring Member dialog box parameters
The
Add/Edit Ring Member
dialog box includes these parameters:Parameter | Description |
---|---|
DHCP Pool | Specifies the name of the Dynamic Host Configuration Protocol (DHCP) IP address pool configured on the switch. A DHCP IP address pool is a range (or pool) of available IP addresses that the switch can assign to connected devices. |
Ring Member Type | Indicates the type of ring member added to the DHCP pool. Allows to select the ring member type.
|
Ring Member | Specifies the order of devices in the ring when the switch is the ring supervisor. The switch is always ring member 1. Available values are 2 to the number of ring members greater than or equal to 2. |
Host Name | For single ring members, defines a descriptive name for the host associated with the ring. Available values are ASCII characters with a maximum length 64. |
IP Address | Defines the IP address assigned to the switch port. The IP address is reserved for the selected port and is not available for normal DHCP dynamic assignment. The IP address must be an address from the pool specified in the DHCP Pool view.Available values are 0 through 255. The first octet should not be 127 and should be less than 224. |
Starting Ring Members | For multiple ring members, specifies Ring Members starting value of the range. |
Ending Ring Members | For multiple ring members, specifies Ring Members ending value of the range. |
Starting IP Address | For multiple ring members, specifies IP Address starting value of the range. |
Ending IP Address | For multiple ring members, specifies IP Address ending value of the range. |
Provide Feedback