- Stratix device properties
Ring X - DHCP view
Use the
Ring X -
DHCP
view to configure Dynamic Host Configuration Protocol (DHCP) for the Device Level Ring (DLR) on the switch.Use the
Ring X -
DHCP
view to:- Indicate whether IP addresses are automatically obtained.
- Select the role of the DLR DHCP server.
- Select the number of ring members.
- View the configured ring members.
- Enable DHCP snooping for the DLR ring.
- Add and edit ring members.
Provide Feedback