Ring X - Members view parameters
The
Ring X - Members
view includes these parameters:Parameter | Description |
---|---|
Ring Member | Shows the order of the devices in the ring. Ring member 1 is always the switch when it is the ring supervisor. |
IP Address | Displays the IP Address of the device. |
MAC Address | Displays the MAC Address of the device. |
Provide Feedback