- Stratix device properties
Ring X - Members view
Use the
Ring X -
Members
view to view information about each device in the ring when the switch is the ring supervisor. The switch is always ring member 1.In the
Ring X -
Members
view, you can:- View the order of the devices in the ring.
- View the IP Address and MAC Address of the devices in the ring.
- Sort the members by IP Address or MAC Address.
TIP:
The parameters in this view are available while online.
Provide Feedback