- Stratix device properties
Ring X - Redundant Gateway view parameters
The
Ring X - Redundant Gateway
view includes these parameters:Parameter | Description |
---|---|
Enable Redundant Gateway | Indicates that the redundant gateway is enabled. The redundant gateway must be enabled before adjusting the parameters. Default: Disabled . |
Advertise Interval | Specifies the time interval in microseconds for the redundant gateway to transmit advertise messages. Acceptable values: 1000 to 100,000 microseconds. Default: 2000 microseconds. |
Advertise Timeout | Specifies the duration of time for nodes to wait before timing out in the absence of received advertise messages. Acceptable values: 2500 to 500,000 microseconds. Default: 5000 microseconds. |
Precedence | Specifies the values for the precedence of the redundant gateway. You can configure multiple gateways and assign each gateway a precedence value. Available values:
|
Enable Sending Learning Update Frame | Indicates that the learning update messages are enabled. Default: Enabled . |
Gateway Uplink Ports | Indicates the uplink ports that are enabled on the redundant gateway. |
Refresh | Retrieves and displays the latest values from the device. |
Set | Sends the settings to the switch. The Enter password dialog box may appear. |
Provide Feedback