- Stratix device properties
Ring X - Redundant Gateway view
Use the
Ring X -
Redundant Gateway
view to configure the redundant gateway when the switch is the ring supervisor.In the
Ring X -
Redundant Gateway
view, you can:- Enable the redundant gateway.
- Specify the advertise interval value.
- Specify the advertise timeout value.
- Assign the precedence.
- Enable sending of the learning update frame.
- Enable the uplink ports for the redundant gateway.
TIP:
The parameters in this view are available while online.
Provide Feedback