Ring X view parameters
The
Ring X
view includes these parameters:Parameters | Description |
---|---|
Network mode | Indicates the network mode. |
Network topology | Displays whether the switch is operating in a DLR or linear network. Available values:
|
Network status | Displays the current status of the network. Available values:
|
Enable supervisor mode | Indicates that the switch is a ring supervisor on the network. If cleared, the supervisor mode is disabled, and the switch is not a supervisor on the network. |
Supervisor status | Displays whether the switch is currently operating as the active ring supervisor or backup ring supervisor. Available values:
Only available when the switch is a ring supervisor. |
Active ring supervisor | Displays the IP address or MAC address of the active ring supervisor. Only available when the switch is operating in a DLR network. |
Active supervisor precedence | Displays the precedence assigned to the active supervisor. The precedence is entered in the Advance Network Configuration dialog box.Only available when the switch is operating in a DLR network. |
Ring faults detected | Displays the number ring faults detected on the network since the last power cycle or counter reset. Only available when the switch is a ring supervisor. |
Last active node on Port 1 | Displays the IP address or MAC ID of the last node the active ring supervisor can communicate with on Port 1 when a ring fault has occurred. Only available when the switch is a ring supervisor. |
Last active node on Port 2 | Displays the IP address or MAC ID of the last node the active ring supervisor can communicate with on Port 2 when a ring fault occurs. Only available when the switch is a ring supervisor. |
Status | Displays the current condition of the ring fault. Available values:
Only available when the switch is a ring supervisor. |
Advanced | Opens the Advanced Network Configuration dialog box to enter the Supervisor precedence number , Beacon interval , and Beacon timeout . |
Reset Counters | Used to reset the ring fault count to zero for the switch. Only available when the switch is a ring supervisor. |
Verify Fault Location | Causes the switch to verify the last node fault location on port 1 and port 2 and update the Last Active Node parameters.The Last Active Node parameters show information from the last fault until you verify the fault location.Only available when the switch is a ring supervisor |
Clear Faults | Used to enable the switch to clear the rapid fault/restore cycles fault. Only available when the switch is a ring supervisor and the fault is Rapid Fault/Restore Cycles. |
Refresh | Retrieves and displays the latest values from the device. |
Provide Feedback