|
Network Topology - Type of network on which the switch is operating Network Status - Current status of the network. Supervisor Mode - Whether the device's Supervisor Mode is enabled or disabled. Configure Supervisor Mode in the Ring view. MAC Address - MAC address of the switch. IP Address - IP address assigned to the switch. Precedence - Precedence currently assigned to the switch. Port 1 - First port on the ring. Port 2 - Second port on the ring.
|
|
Mode - Whether the device's Supervisor Mode is enabled or disabled. Configure Supervisor Mode in the Ring view. Status - Status of the active ring supervisor. Only available when Supervisor Mode is enabled. MAC Address - MAC address of the active ring supervisor. IP Address - IP address assigned to the active ring supervisor. Beacon Interval - Frequency that the active ring supervisor transmits a beacon frame through both of its ring ports. Default interval is 400 µs. Available only when Supervisor Mode is enabled. Beacon Timeout - Amount of time the ring nodes wait before timing out in the absence of received beacon frames. The timeout value must be at least 2 times the Beacon Interval value but cannot exceed 500,000 µs. Available only when Supervisor Mode is enabled. Precedence - Precedence currently assigned to the active ring supervisor. Ring Protocol VLAN ID - VLAN ID to use in the ring protocol message. Available only when Supervisor Mode is enabled.
|
|
Redundant Gateway - Whether the redundant gateway is enabled. Status - Current condition of the ring fault. Advertise Interval - Time interval in microseconds for the gateway to transmit advertise messages. Advertise Timeout - Duration of time in microseconds for nodes to wait before timing out in the absence of received advertise messages. Precedence - Precedence currently assigned to the redundant gateway. Sending Learning Frame - Whether learning update messages are enabled. Uplink Port 1 - Port number used for uplink port 1 on the redundant gateway and whether it is enabled. Uplink Port 2 - Port number used for uplink port 2 on the redundant gateway and whether it is enabled.
|
|
MAC Address - MAC address of the active redundant gateway. IP Address - IP address assigned to the active redundant gateway. Precedence - Precedence currently assigned to the active redundant gateway.
|