DHCP Address Assignment view parameters

DHCP Address Assignment view parameters

The
DHCP Address Assignment
view includes these parameters:
TIP:
If you delete all the rows of pools in the
DHCP Pools
view and select
Refresh
, the
Pool
name becomes empty.
Parameter
Description
Port
Displays the ports available for the configuration. For example, Gi1/1, Gi1/2, Fa1/1, Fa1/2.
Pool
Specifies the pool names from the DHCP IP address pool that corresponds to the instances available in the switch.
IP Address
Specifies the IP address assigned to the switch port. The format is a 32-bit numeric address written as four numbers separated by periods (for example, 255.255.255.255). The number range is between 0 and 255 (from 1 through 244).
The IP address that you assign is reserved for the selected port and is not available for normal DHCP dynamic assignment. The IP address must be an address from the pool specified in the DHCP
Pool
field.
Refresh
Retrieves and displays the latest values from the device.
Set
Sends the settings to the switch. The
Enter password
dialog box may appear.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.