DHCP Pools view parameters
The
DHCP Pools
view includes these parameters:Parameter | Description |
---|---|
Enable Dynamic Host Configuration Protocol (DHCP) | Indicates whether the DHCP pool is enabled or disabled. The values are obtained from the switch and displayed only when the DHCP is enabled. |
Enable DHCP Snooping | Indicates whether Dynamic Host Configuration Protocol (DHCP) snooping is enabled or disabled. |
![]() | Opens the Add/Edit DHCP Pool dialog box to create a new DHCP pool. |
![]() | Opens the Add/Edit DHCP Pool dialog box to edit the DHCP pool properties. |
![]() | Deletes the currently selected DHCP pool row. All persistent addresses associated with the selected DHCP pool are deleted as well. |
Name | Specifies the name of the DHCP IP address pool configured on the switch. A DHCP IP address pool is a range (or pool) of available IP addresses that the switch can assign to connected devices. |
Starting IP Address | Displays the starting IP address that defines the range of addresses in the DHCP IP address pool. |
Ending IP Address | Displays the ending IP address that defines the range of addresses in the DHCP IP address pool. |
Preassigned Addresses Only | Indicates whether the IP address is preassigned for the selected port and is not available for normal DHCP dynamic assignment. The IP address must be an address from the pool specified in the DHCP Address Assignment view in the DHCP Pool field. |
DHCP Snooping | Indicates whether broadcast of DHCP requests are restricted beyond the connected switch or not. If enabled, devices only receive address assignments from the connected switch. This option is available on VLAN interfaces. |
Refresh | Retrieves and displays the latest values from the device. |
Set | Sends the settings to the switch. The Enter password dialog box may appear. |
Provide Feedback