- Stratix device properties
DHCP Pools view
Use the
DHCP Pools
view to view the Dynamic Host Configuration Protocol (DHCP) address pool information for the switch (from 0 through 15 pools can be displayed). When the DHCP is enabled, the information is gathered directly from the switch - each row represents a single instance and instance value may not be consecutive.Use the
DHCP Pools
view to:- Enable DHCP
- Enable DHCP snooping
- View DHCP address pool information
- Create a new DHCP pool
- Edit the properties of an existing DHCP pool
- Delete an existing DHCP pool
TIP:
The data is only displayed when the device is online and
Enable Dynamic Host Configuration Protocol (DHCP)
is selected.Provide Feedback