- Stratix device properties
Delete NAT Instance confirmation dialog box
When the NAT instance is deleted, all of the translation parameters associated with the NAT instance are also deleted.
To continue, do one of these actions:
- SelectDeleteto delete the instances from the switch and close the dialog box.
- SelectCancelto close the dialog box without deleting the instances.
Provide Feedback