- Stratix device properties
NAT Diagnostics - InstanceX dialog box parameters
The
NAT Diagnostics - InstanceX
dialog box contains these parameters.Parameters | Description |
---|---|
Current Active Translations | Displays the number of translations that have occurred within the last 90 seconds across all NAT instances. |
Total NAT Translated Packets | Displays the total number of packets that have been translated for this NAT instance. |
Total Private to Public Address Translations | Displays the total number of private-to-public translations for this NAT instance. |
Total Public to Private Address Translations | Displays the total number of public-to-private translations for this NAT instance. |
Total Translations | Displays the total number of private-to-public and public-to-private translations for this NAT instance. |
ARP Fixup Packets | Displays the number of ARP (Address Resolution Protocol) packets that have been fixed up for this NAT instance. |
ICMP Fixup Packets | Displays the number of ICMP (Internet Control Message Protocol) packets that have been fixed up for this NAT instance. |
Total Fixup Packets | Displays the number of ARP and ICMP packets that have been fixed up for this NAT instance. |
Blocked Non-Translated Traffic Packets | Displays the number of packets with untranslated traffic that were blocked for this NAT instance. |
Pass-Through Non-Translated Traffic Packets | Displays the number of packets with untranslated traffic that were passed through for this instance. |
Blocked Multicast Traffic Packets | Displays the number of packets with multicast traffic that were blocked for this NAT instance. |
Pass-Through Multicast Traffic Packets | Displays the number of packets with multicast traffic that were passed through for this NAT instance. |
Blocked IGMP Traffic Packets | Displays the number of packets with IGMP (Internet Group Managed Protocol) traffic that were blocked for this NAT instance. |
Pass-Through IGMP Traffic Packets | Displays the number of packets with IGMP traffic that were passed through for this NAT instance. |
Private to Public Translations | Opens the Private to Public Translations dialog box to view private-to-public translation diagnostics for the instance. |
Public to Private Translations | Opens the Public to Private Translations dialog box to view public-to-private translation diagnostics for the instance. |
Refresh | Retrieves and displays the latest values from the device. |
Clear Diagnostics | Clears the diagnostic totals for this NAT instance. |
Provide Feedback