Add/Edit NAT Instance - Overview view parameters

Add/Edit NAT Instance - Overview view parameters

Use the
Overview
view includes these parameters.
Parameter
Description
Name
Displays the NAT instance name. The field is not editable when editing an existing instance.
Private to Public
New Entry
Creates a new entry in the Private to Public NAT Table.
Any row that has not yet been sent to the switch is denoted by an asterisk in the left column.
Delete
Deletes the table entry.
Private
Displays the unique private IP address.
Public
Displays the unique public IP address.
Subnet Mask
Displays the subnet mask.
Gateway Translation
Enables devices on the public subnet to communicate with devices on the private subnet.
Public
Indicates the default gateway address of the Layer 3 switch or router connected to the switch's uplink port.
Private
Indicates the unique IP address to represent the Layer 3 switch or router on the private network.
VLAN Association
VLAN
Displays the VLAN list.
Gi1/1
Indicates that the VLAN on port Gi1/1 is assigned to this NAT instance. If cleared, the VLAN is not assigned to this NAT instance.
By default, all VLANs not used by other instances are selected. VLANs used by other instances are disabled.
Gi1/2
Indicates that the VLAN on port Gi1/2 is assigned to this NAT instance. If cleared, the VLAN is not assigned to this NAT instance.
By default, all VLANs not used by other instances are enabled and available to select. VLANs used by other instances are disabled.
Gi1/3
Indicates that the VLAN on port Gi1/3 is assigned to this NAT instance. If cleared, the VLAN is not assigned to this NAT instance.
By default, all VLANs not used by other instances are enabled and available to select. VLANs used by other instances are disabled.
Gi1/4
Indicates that the VLAN on port Gi1/4 is assigned to this NAT instance. If cleared, the VLAN is not assigned to this NAT instance.
By default, all VLANs not used by other instances are enabled and available to select. VLANs used by other instances are disabled.
Refresh
Retrieves and displays the latest values from the device.
Set
Sends the settings to the switch. The
Enter password
dialog box may appear.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.