NAT view parameters

NAT view parameters

The
NAT
view includes these parameters:
Parameter
Description
Network Address Translation (NAT) Instances
Instance Name
Displays the unique name of the NAT instance.
Gi1/1 VLAN's
Displays the VLANs assigned to the NAT instance on port Gi1/1.
Gi1/2 VLAN's
Displays the VLANs assigned to the NAT instance on port Gi1/2.
Gi1/3 VLAN's
Displays the VLANs assigned to the NAT instance on port Gi1/3.
Gi1/4 VLAN's
Displays the VLANs assigned to the NAT instance on port Gi1/4.
Diagnostics
Opens
NAT Diagnostics
to view diagnostic information about an instance.
Global Diagnostics
Current Active Translations
Displays the total number of translations that occurred within the last 90 seconds across all NAT instances.
Total Translations
Displays the total number of translation across all NAT instances.
Total Translated Packets
Displays the total number of translations across all NAT instances.
Total Untranslated Packets
Displays the total number of packets that have been bypassed and dropped across all NAT instances.
Add
Opens
Add/Edit NAT Instance
to create a NAT instance.
Edit
Opens
Add/Edit NAT Instance
to edit the configuration of a NAT instance.
Delete
Deletes the NAT instance.
When the NAT instance is deleted, all of the translation parameters associated with the NAT instance are also deleted.
Refresh
Retrieves and displays the latest values from the device.
Set
Sends the settings to the switch. The
Enter password
dialog box may appear.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.