Private to Public Translations - InstanceX dialog box parameters

Private to Public Translations - InstanceX dialog box parameters

The
Private to Public Translations - InstanceX
dialog box includes these parameters:
Parameter
Description
Private
Displays the existing address for a device on the private subnet.
Public
Displays a unique public address that represents the corresponding device on the private subnet.
Subnet
Indicates whether the translation is part of a Subnet entry type.
Number of Packets
Displays the number of packets for each translation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.