Public to Private Translations - InstanceX dialog box parameters

Public to Private Translations - InstanceX dialog box parameters

The
Public to Private Translations - InstanceX
dialog box includes these parameters:
Parameter
Description
Public
Displays the unique IP address on the public subnet that represents the corresponding IP address on the private subnet.
Private
Displays the IP address on the private subnet that was changed to a unique IP address on the public subnet.
Subnet
Indicates whether the translation is part of a Subnet entry type.
Number of Packets
Displays the number of packets for each translation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.