Advanced dialog box parameters

Advanced dialog box parameters

The
Advanced
dialog box contains these parameters.
Parameter
Description
Traffic Permits
The types of incoming and outgoing packets that are not handled by NAT. Available values:
  • Multicast
  • IGMP
Incoming
Specifies how to handle each type of incoming packet. Available values:
  • Blocked
    (default) – drop the packets
  • Pass-Through
    – permit the packets to pass across the NAT boundary
Outgoing
Specifies how to handle each type of outgoing packet. Available values:
  • Blocked
    (default) – drop the packets
  • Pass-Through
    – permit the packets to pass across the NAT boundary
Fixup Packets
Specifies the fixup protocols to be enabled. Available options are:
  • ARP
    - Indicates that the fix up protocols for ARP (Address Resolution Protocol) are enabled. If cleared, the fix up protocols are disabled.
  • ICMP
    - Indicates that the fix up protocols for ICMP (Internet Control Message Protocol) are enabled. If cleared, the fix up protocols are disabled.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.