- Stratix device properties
Gateway Address view
Use this view to enable devices on the public subnet to communicate with devices on the private subnet.
TIP:
When multiple VLANs are assigned to a port, you do not need to set gateway addresses.
In the
Gateway Address
view, you can enter a:- Public gateway address for a NAT instance.
- Private gateway address for a NAT instance.
TIP:
The parameters in this view are available while online.
Provide Feedback