Instance Name and Ports view parameters

Instance Name and Ports view parameters

The
Instance Name and Ports
view contains the following parameters.
Parameter
Description
NAT Instance Name
Specifies the unique name of the NAT instance.
Port Type
Specifies the port type. Available options are:
  • Uplink Ports Only (Te1/25 - Te1/28)
    - Indicates that the uplink ports (Te1/25-28) can be selected.
  • Downlink Ports Only (Gi1/1 - Gi1/24)
    - Indicates that the downlink ports (Gi/1-6 and Gi/13-18, Gi/7-12 and Gi/19-24) can be selected.
Select 4 or fewer ports
Indicates the ports available for the new NAT instance. You can select up to four ports for each section. If a port has been selected in another NAT instance, it is not available.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.