Associate VLANs view parameters

Associate VLANs view parameters

The
Associate VLANs
view contains these parameters.
Parameter
Description
VLAN
Indicates whether the VLAN is assigned to the port. After assigned to a port, VLAN attributes are translated for that port.
<Port>
Displays the ports that were selected in the
Instance Name and Ports
view.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.