- Stratix device properties
NTP Client view parameters
The
NTP Client
view includes these parameters.Parameter | Description |
---|---|
Network Time Protocol (NTP) Enabled | When the switch is online, this value shows whether NTP is enabled on the switch. When the switch is offline, this value is blank. If the value shows Yes , the other parameters in the NTP Client view show values or are enabled.If the value shows No or blank, the other parameters in the NTP Client view show blank values or are disabled. |
System Poll Interval | Shows the system poll interval. The value is 8-12700 seconds. |
Synchronized | Shows whether the switch clock is synchronized. |
Current Time | Shows the current time on the switch. |
NTP Servers | |
![]() | Opens the Add NTP Server dialog box. |
![]() | Select to delete the selected NTP server address. |
NTP Server Address | Shows the NTP server addresses. |
Preferred Server | Specifies whether the NTP server is preferred and provides the synchronization. The available values are:
|
NTP Status | Shows the NTP status of the NTP servers. The available values are:
|
Stratum of Clock | Shows the stratum of clock, which indicates how many NTP hops away a device is from an authoritative time source. The value is from 0 through 16. |
Time Since Last Update | Shows the time since last update in seconds. |
Refresh | Retrieves and displays the latest values from the device. |
Set | Sends the settings to the switch. The Enter password dialog box may appear. |
Provide Feedback