- Stratix device properties
Network view parameters
Use the
Network
view to view information about the Device Level Ring (DLR) network.Parameter | Description |
---|---|
Network mode | Indicates that the device profile is online to a Device Level Ring (DLR) capable device. |
Network topology | Displays the current network topology as either:
|
Network status | Displays the current network status as:
|
Supervisor | |
Enable supervisor mode | Indicates that the device is configured as a supervisor on the network. If cleared, Supervisor Mode is disabled, and the device is not a supervisor on the network. |
Supervisor status | Displays the status of the supervisor. Only available when Supervisor Mode is enabled. Available values:
|
Active ring supervisor | Displays the IP Address or MAC Address of the Active Ring Supervisor. Only available when the device is in a Ring network. |
Active supervisor precedence | Displays the precedence currently assigned to the active ring supervisor. Only available when the device is in a Ring network. |
Advanced | Opens Advanced Network Configuration to configure advanced network properties. |
Ring Fault | |
Ring faults detected | Displays the number of ring faults detected on the network since the last power cycle or counter reset. Only available when the device is a ring supervisor. |
Last active node on Port 1 Last active node on Port 2 | Displays the IP or MAC Address for the last active node on Port 1 or Port 2 when the device is the Active Ring Supervisor on the network. |
Reset Counter | Used to reset the device's ring fault count to zero. Only available when the device is a ring supervisor. |
Verify Fault Location | Causes the device to verify the last node fault location on port 1 and port 2 and update the last active node parameters. The last active node parameters show information from the last fault until you verify the fault location. Only available when the device is a ring supervisor. |
Port Buffer Utilization | |
Port 1 Port 2 | Displays the percentage of the buffer that is being used for port 1 and port 2. |
Device port | Displays the percentage of the device port that is being used. |
Refresh | Retrieves and displays the latest values from the device. |
Provide Feedback