Network view

Network view

Use the
Network
view to view the network information. If the device profile is online to a DLR capable device, use these settings to:
  • View whether the network is operating in Linear/Star or Ring network.
  • View the current status of the network.
  • Enable the device to be a supervisor on the network.
  • View the address of the active ring supervisor and the active supervisor precedence.
  • View information about the ring faults such as the number of ring faults and the status of the ring faults.
  • Reset the ring fault count to zero.
TIP:
This information is only available when online, and there is no communication error in the device profile.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.