Overview view parameters

Overview view parameters

The
Overview
view includes these parameters.
Parameter
Description
Revision
Displays the device major and minor revisions.
Electronic keying
Displays the electronic keying used for the device. Electronic keying compares the device defined in the project to the installed device. If keying fails, a fault occurs.
Valid values include:
  • Exact Match
  • Compatible Module
  • Disable Keying
For detailed information on Electronic keying, see Electronic Keying in
Logix5000
Control Systems Application Technique
, publication LOGIX-AT001.
Connection
Displays the type of I/O connection to use between the device and the controller.
Device definition
Opens
Device definition
to change the revision, electronic keying, and other device specific values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.