- Stratix device properties
Port Configuration view parameters
The
Port Configuration
view includes these parameters:Parameter | Description |
---|---|
Port | Displays the port to which this configuration applies. The port number includes the port type (Fa for Fast Ethernet, Gi for Gigabit Ethernet, or Te for Ten Gigabit), the base or expansion device number (1 for the base, 2 for the first expansion device, or 3 for the second expansion device), and the specific port number. For example:
The base and expansion device number is only applicable for Stratix 8000/8300 switches. |
Enable | Indicates that the port is enabled. If cleared, the port is disabled. We recommend disabling the port if the port is not in use and is not attached to a device, and to troubleshoot a suspected unauthorized connection. Not available in offline mode. |
Link Status | Displays the port’s link status as Active or Inactive . |
Auto-Negotiate | Indicates that the port and end-device will auto-negotiate the link speed and duplex mode. If cleared, manually select the desired port speed and duplex mode. Not available in offline mode. |
Speed Selected Speed Current | The operating speed of the port. Speed is blank when the port is not connected and not available when Auto-Negotiate is enabled.Possible speed for different ports are:
The available speed values for each port depend on the device:
|
Duplex Selected Duplex Current | Specifies the duplex mode of the port. The available values for each port are:
Duplex is not available when Auto-Negotiate is enabled. |
Port Diagnostics | Opens the dialog box for diagnostics information. |
Refresh | Retrieves and displays the latest values from the device. |
Set | Sends the settings to the switch. The Enter password dialog box may appear. |
Provide Feedback