Port Security view parameters

Port Security view parameters

The
Port Security
view includes these parameters:
Parameter
Description
Port
Indicates the port selected for configuration. The port number includes the port type (Fa for Fast Ethernet and Gi for Gigabit Ethernet) and the specific port number. For example:
  • Gi1/1 is Gigabit Ethernet port 1.
  • Gi1/2 is Gigabit Ethernet port 2.
  • Fa1/1 is Fast Ethernet port 1.
Enable
Indicates that port security is enabled. If cleared, port security is disabled.
MAC Addresses
Allowed
Specifies the number of MAC addresses allowed to connect to the port. This number must be between 1 and 80.
MAC Addresses
Dynamic
Displays the number of dynamic (not statically defined) MAC addresses currently connected to the port.
MAC Addresses
Static
Displays the number of static MAC addresses allowed for the port. These can be configured using Device Manager Web Interface or CLI.
Refresh
Retrieves and displays the latest values from the device.
Set
Sends the settings to the switch. The
Enter password
dialog box may appear.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.