Port Diagnostics dialog box parameters

Port Diagnostics dialog box parameters

The
Port Diagnostics
dialog box includes these parameters:
Parameter
Description
Unit
Indicates the unit where the port resides.
Interface Counters
These status elements allow you to view status of octets received and sent, and packets received and sent.
  • Octets inbound
    - the number of octets received by the port.
  • Octets outbound
    - the number of octets sent by the port.
  • Unicast packets inbound
    - the number of unicast packets received by the port.
  • Unicast packets outbound
    - the number of unicast packets sent by the port.
  • Non-unicast packets inbound
    - the number of multicast packets received by the port.
  • Non-unicast packets outbound
    - the number of multicast packets sent by the port.
  • Packets discards inbound
    - the number of inbound packets that were discarded.
  • Packets discards outbound
    - the number of outbound packets that were discarded.
  • Packets with errors inbound
    - the number of inbound packets that contain errors.
  • Packets with errors outbound
    - the number of outbound packets that contain errors.
  • Unknown protocol packets inbound
    - the number of inbound packets with unknown protocols.
Media Counters
Indicates the counters that allow you to view the status of these elements:
  • Alignment errors
    - the number of frames received that are not an integral number of octets in length.
  • FCS errors
    - Frame Check Sequence errors. The number of frames received that do not pass the FCS check.
  • Single collisions
    - the number of single collisions.
  • Multiple collisions
    - the number of multiple collisions.
  • SQE test errors
    - the number of times that the SQE TEST ERROR message is generated.
  • Deferred transmissions
    - count of transmissions deferred by busy network.
  • Late collisions
    - the number of late collisions.
  • Excessive collisions
    - the number of frames for which transmission fails due to excessive collisions.
  • MAC transmit errors
    - the number of frames that failed to transmit due to an internal MAC sublayer transmit error.
  • MAC receive errors
    - the number of frames that failed to be received due to an internal MAC sublayer receive error.
  • Carrier sense
    - the number of times the carrier sense condition was lost or never asserted when attempting to transmit a frame.
  • Frame too long
    - the number of frames received that exceed the maximum permitted frame size.
Reset counters
Resets the counters to zero.
Reset counters
is not available while offline.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.