Port Thresholds view parameters

Port Thresholds view parameters

The
Port Thresholds
view includes these parameters.
Parameter
Description
Port
Indicates the port selected for configuration. The port number includes the port type (Fa for Fast Ethernet and Gi for Gigabit Ethernet) and the specific port number. For example:
  • Gi1/1 is Gigabit Ethernet port 1.
  • Gi1/2 is Gigabit Ethernet port 2.
  • Fa1/1 is Fast Ethernet port 1.
Incoming: Unicast
Enable
Indicates that the
Unicast
Threshold
and
Units
are enabled. If cleared, the
Unicast Threshold
and
Units
are disabled and zero (0) is sent to the switch.
Incoming: Unicast
Threshold
The unicast value threshold after you choose the unit of measurement.
If
Units
is set to pps or bps, the value is between 1 and 4,294,967,295.
If
Units
is set to %, the value is between 1 and 99.
Incoming: Unicast
Units
The unicast threshold unit of measurement. The available values for each port are:
  • pps (packets per second)
  • bps (bits per second)
  • % (percentage of total available bandwidth of the port)
Incoming: Multicast
Enable
Indicates that the
Multicast
Threshold
and
Units
are enabled. If cleared, the
Multicast Threshold
and
Units
are disabled and zero (0) is sent to the switch.
Incoming: Multicast
Threshold
The multicast threshold value after you choose the unit of measurement.
If
Units
is set to pps or bps, the value is between 1 and 4,294,967,295.
If
Units
is set to %, the value is between 1 and 99.
Incoming: Multicast
Units
The multicast threshold unit of measurement. The available values for each port are:
  • pps (packets per second)
  • bps (bits per second)
  • % (percentage of total available bandwidth of the port)
Incoming: Broadcast
Enable
Indicates that the
Broadcast Threshold
and
Units
are enabled. If cleared, the
Broadcast Threshold
and
Units
are disabled and zero (0) is sent to the switch.
Incoming: Broadcast
Threshold
The broadcast threshold value after you choose the unit of measurement.
If
Units
is set to pps or bps, the value is between 1 and 4,294,967,295.
If
Units
is set to %, the value is between 1 and 99.
Incoming: Broadcast
Units
The broadcast threshold unit of measurement. The available values for each port are:
  • pps (packets per second)
  • bps (bits per second)
  • % (percentage of total available bandwidth of the port)
Outgoing: All Traffic
Enable
Indicates that the
All Traffic
Thresholds
are enabled. If cleared, the
All Traffic Thresholds
are disabled and zero (0) is sent to the switch.
Outgoing: All Traffic
Threshold
The
All Traffic
thresholds value . The value is between 10 and 90.
Outgoing: All Traffic
Units
Shows % as the unit of measurement for the
All Traffic
thresholds.
Refresh
Retrieves and displays the latest values from the device.
Set
Sends the settings to the switch. The
Enter password
dialog box may appear.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.