- Stratix device properties
Save/Restore view parameters
The
Save/Restore
view includes these parameters:Parameter | Description |
---|---|
Exchange Configuration with Switch | |
Upload | Uploads the the config.text file and vlan.dat file from the switch to the project. |
Download | Downloads the config.text file and vlan.dat file from the project to the switch. |
Import/Export Configuration | |
Import | Opens Import to enter the config.text and vlan.dat files that you want to import from your computer to the project. |
Export | Opens Export to enter the config.text and vlan.dat files that you want to export from the project to your computer. |
Provide Feedback