- Stratix device properties
Connection interruption
Downloading a configuration to the switch resets the switch and temporarily interrupts (break) all connections to the switch.
Ensure a connection interruption at this time is acceptable before proceeding.
To download the configuration to the switch
- If a connection interruption is acceptable at this time, inDownload Confirmation, selectYes. Otherwise, selectNoto cancel the operation.
Provide Feedback