DLR IP address is invalid

DLR IP address is invalid

The DLR IP address is not within the defined range of the DHCP pool. Enter a valid value from 0 through 255 for each octet. The first octet should not be 127 and should be less than 224.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.