- Stratix device properties
Duplicate DLR IP address
The DLR IP address already exists. Enter a valid value from 0 through 255 for each octet. The first octet should not be 127 and should be less than 224.
Provide Feedback