Invalid private IP address for the selected subnet mask
Invalid starting private IP address for the selected subnet mask. Enter a valid IP address that corresponds to the size of the subnet mask.
Subnet Mask | Starting Private Subnet Address |
255.255.0.0 | The last two octets must be 0. EXAMPLE: 10.200.0.0 |
255.255.255.0 | The last octet must be 0. EXAMPLE: 10.200.1.0 |
255.255.255.128 | The last octet must be 0 or 128. EXAMPLE: 10.200.1.0 or 10.200.1.128 |
255.255.255.192 | The last octet must be one of these numbers: 0, 64, 128, 192. EXAMPLE: 10.200.1.64 |
255.255.255.224 | The last octet must be one of these numbers: 0, 32, 64, 96,128, 160, 192, 224. EXAMPLE: 10.200.1.32 |
255.255.255.240 | The last octet must be one of these numbers: 0, 16, 32, 48, 64, 80, 96, 112, 128, 144, 160, 176, 192, 208, 224, 240. EXAMPLE: 10.200.1.16 |
Provide Feedback