Invalid public IP address

Invalid public IP address

The starting public IP address is blank or invalid. The valid range is:
  • Class A (Netid.hostid.hostid.hostid): 1.0.0.0–126.255.255.255
  • Class B (Netid.Netid.hosid.hostid): 128.0.0.0–191.255.255.255
  • Class C (Netid.Netid.Netid.hostid): 192.0.0.0–223.255.255.255
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.