- Stratix device properties
Invalid ring member
The ring member (single) or the starting ring member (multiple) is blank or invalid. Enter a valid value from 2 through the number of ring members greater than or equal to 2.
Provide Feedback