Invalid total power supported value

Invalid total power supported value

The total power support value is blank or out of range. Enter a value based on the power source and the Stratix switch type.
  • For 5400 Stratix switches, the value range is from 4 W through 125 W.
  • For 5800 Stratix switches, the value range is from 4 W through 240 W.
  • For 5800 plus Stratix switches, the value range is from 4 W through 480 W.
  • For 5410 and other Stratix switches, the value range is from 4 W through 130 W.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.