- Stratix device properties
IP address already assigned to port
The IP address entered for a port already has an IP address assigned.
To maintain the currently assigned IP address for the specified port, select
Cancel
.To change the currently assigned IP address for the specified port, select
OK
(this removes the previously assigned IP address from the port).Provide Feedback