IP address over range

IP address over range

For most Stratix switches, you entered an invalid range based on the starting private/public IP address. The range exceeds Class C boundaries. For example, if the starting private IP address is 112.120.100.200 and the range is 100, the last octet exceeds the maximum of 255.
For a 5410 Stratix switch, you entered an invalid count based on the private/public IP address. The count exceeds Class C boundaries.
Enter a new value for range or count.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.