Subnet mask IP address too small
The subnet mask IP address is smaller than 255.0.0.0. By default, the DHCP pool network IP address is adjusted to the starting IP address allowed by the subnet mask.
Provide Feedback